Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...
Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...
This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...
This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...
Can I get wider bandwidth than 200 Hz?
No. The ADXL362 is capable of operation up to a 400 Hz output data rate (ODR) or 200 Hz bandwidth.