ADXRS646 Null Output Over Temperature

Hi there,

I'm working on a system which uses the ADXRS646-EP to measure the rate of rotation about one axis in a vehicle.  We have a circuit to cancel the null output which we tune during production, such that the system output is zero for zero rotation at 25°C.  However, we're concerned that the null drift over temperature could result in an apparent output as high as ~10°/sec if the system is operating near the edge of its temperature range.  It's possible that we could modify the system to zero the output at start-up, but this wouldn't account for any null drift if the system were to start cold and warm up during operation, for example.  With that in mind, a few questions:

-Is there a way that we can make use of the TEMP output to compensate for temperature drift without individually characterizing each gyro?
-Can we reduce the measurement range from ±250°/sec?  We only need about ±50°/sec for this application; if we were able to increase the sensitivity by a factor of 5, the apparent rotation caused by temperature drift would be reduced by a factor of 5 as well.
-Is there a different part that you'd recommend for this application, or anything else that you can think of that might be able to help us out?

Thanks,

Kyle

Parents Reply Children
No Data