Has anybody ever tried to measure the Earth rotation with ADIS16460?

I tried to check the possibilty of the Earth rotation rate measure. I cannibalized old HDD to prepare the rotating table, attached the device to the plate, and performed the series of recordings, turning the device by 180° every 75 seconds, after 10 rotations the results were calculated. 15 series of 10 rotations each were recorded.

Certainly i could catch only horizontal component (vertical is invisible due to linear acceleration effect), i.e. i need to multiply the value by the cos(55.75°). The latitude of my office is 55.75°.

Can you bet the average measured value and STDEV for 15 series of 10 rotations each?

Do you think this research worth writing an artice?

Parents
No Data
Reply
  • Test no

    Sensor no

    Active axis

    Value measured

    Relative to actual

    1

    1

    X

    ±0.002176°/s

    0.924

    2

    1

    X

    ±0.002727°/s

    1.160

    3

    1

    Y

    ±0.002235°/s

    0.951

    4

    1

    X

    ±0.002408°/s

    1.024

    5

    1

    Y

    ±0.002527°/s

    1.075

    6

    1

    Y

    ±0.003327°/s

    1.415

    7

    1

    Y

    ±0.002918°/s

    1.241

    8

    1

    X

    ±0.003391°/s

    1.442

    9

    1

    X

    ±0.002346°/s

    0.998

    10

    2

    Y

    ±0.002116°/s

    0.900

    11

    2

    X

    ±0.002533°/s

    1.077

    12

    2

    X

    ±0.002394°/s

    1.018

    13

    2

    Y

    ±0.002028°/s

    0.862

    14

    2

    X

    ±0.002095°/s

    0.891

    15

    2

    Y

    ±0.002287°/s

    0.972

    16

    2

    Y

    ±0.002189°/s

    0.931

     

     

     

     

     

    average

     

    average

    ±0.002481°/s

    1.055

     

     

    STDEV

    ±0.000403°/s

     

     

    Actual value computed as 360°/86164*cos(55.75°)=0.002351°/s

Children
No Data