Post Go back to editing

[ADXL354-ADXL355] Frequency response for seismic purposes

Hi to all, I don't know if someone would be already interested about using these MEMS accelerometers for seismic purposes (or has already done this).....
I have some doubts about frequency response.

page 3 of datasheet:

resonant frequency (1) = 2.4 kHz

(1) sensor characteristic [...] an analog 1.5kHz (-6dB) that cannot be bypassed limits actual output response

page 23 of datasheet:

The ADXL354/ADXL355 use an analog, low-pass, antialiasing filter to reduce noise and limit banwidth.

The ADXL355 provides further digital filtering options [...]

The analog, low-pass antialiasing filter [...] provides 1,5kHz bandwidth where output response is attenuated by 50%. The shape of filter response in the frequency domain is sinc3 filter.

So I understand both have got same internal low-pass filter, but in graphs shown in fig. 7, 8, 9 for ADXL354 shows 2400 Hz peak (I suppose resonance frequency), so without low-pass analog filter.....?????


1) I need poles and zeros to simulate frequency response of filter (usually seismic sensors have given poles and zeros from which  take out bode diagram for further analysis for compensation in terms of magnitude and phase). Is there a way to know parameters (poles and zeros) to do sensor simulation?

Talking about ADXL355:

Additional digital filtering [...] consist of low-pass digital decimation filter.
[...]
The first stage is fixed decimation filter with a 4kHz ODR with a low-pass filter cutoff (50% reduction in output response) at about 1kHz.

[...] second stage decimation filter is used for 2kHz output data rate and below [...]
Figure 60 shows the low-pass filter response with 1kHz corner (4kHz ODR) for ADXL355.

So first stage is decimation (low-pass) filter with sampling frequency of 4kSPS, I suppose the one in fig. 60 (not taking care of analog filter, right?), so why sampling frequency of fig. 60 looks like 20 kSPS?
I'm a bit confused.....

2) are there available digital filter (stage 1 and 2) coefficients or instructions to replicate model in Matlab?

Thanks.

Parents
  • Goodmorning Anthony, thanks for answer but keep in mind this for my purposes:
    I'm aware seismic instruments (sensors and dataloggers) work at low frequencies with much less noise, but my target is design a cost-effective (compared to professional instruments such as Nanometrics, Kinemetrics, Quanterra, Sara and so on) device.

    Obviously with "lower" performances

    Of course I can buy professional accelerometer for seismic application with no noise, but it works at low frequencies, or  I can buy narrow band accelerometer, with higher cost and high noise.

    My purpose is to compare professional seismic accelerometers (such Titan and Episensor) and MEMS based seismic accelerometers (GeoSig) with commercial MEMS (in sensor arrays such Suricat or stand-alone such Raspberry shields).

    I can get PGA (peak gain acceleration) values during an earthquake from several 4$ MEMS (180ug/sqrt(Hz)), but it would be better if I find for same price (35$ in this aapplication for me stands for "more or less") a 50ug/sqrt(Hz) so I can detect smaller events.

    At same time, I can use MEMS accelerometer for monitor earthquake effects on a building, installing one device for every floor. Which is the difference between a "cheap" LIS344ALH (just for example, to take a "concurrent" sensor) and an ADXL354 (with lower noise)?

    How much will noise affects results on monitoring building?
    How far are results obtained from a professional accelerometer (Titan SMA) and a MEMS based device?
    Could I use a MEMS based device instead professional one? If so, keep in mind for the same price of Titan SMA I can fill a building with at least 10-15 devices or, for same budget, monitor 10-15 buildings instead only one.

    So you can understand comparing "on the fly" professional instruments and cost-effective deevices is not so easy just reading sensor datasheet.
    Then you can see comparing different sensors on shake-table will give you different results in terms of phase delay (and so in terms of waves analysis) even if transfert function (magnitude) is more or less the same (that's why researchers who will perform analysis asks me poles/zeros and/or filter coefficients).

    Ok, let's come back to ADXL: ADXL354 is perfect for our characteristics in terms of selectable range, frequency range (0-1000Hz), cost and self noise.
    I selected this MEMS also because same "core" is available in both analog and digital version.

    As you correctly said in your answer I can add an external ADC for ADXL354, but this means I can increase space and components number: between LIS344ALH (I use this as example because I've already seen it in seismic devices) with external signal conditioning and ADC, and ADXL355, which do you think I'll prefer if I need to design a board for Intel Edison?

    I understand you can't tell me factory "secrets" of ADXL sensors, but for my purpose just "take a look to datasheet plots" doesn't help me so much.

    For ADXL001 (I've found a thread in this forum) it's reported on datasheet both resonant frequency and quality factor, so there was a Matlab script for modeling accelerometer core.

    I used same script with no success.

    s=tf('s');
    wao=2*pi*2400;
    qao= 10;
    qao= 11*1.276;

    NUMa=wao^2;
    DENa=[1 wao/qao wao^2];
    Ha=tf(NUMa,DENa);

    freq(1:5000)=1:5000;
    omega(1:5000)=2*pi*freq(1:5000);
    [ma,pa]=bode(Ha,omega);
    Ma(1:5000)=(abs(ma(1,1:5000)));


    % reference from ADXL354 graph
    x_ref=[1500,2132, 2400,2795, 3000, 4000, 5000];
    y_ref=[1.09,2, 6.7, 2,1, 0.2, 0.1];


    loglog(freq,Ma,'-b',x_ref,y_ref,'g*', 1500, 2*1.09, 'rx');

    grid on;
    hold on
    ylim([0.01 10]);
    xlim([10 5000]);
    ylabel('Xout [g]');
    xlabel('FREQUENCY [Hz]');
    title('ADXL354 frequency response for X-Axis');
    legend('hypothetical accelerometer core (Wr=2.4kHz, Q=11)', 'ADXL354 datasheet', 'core value (@1500 Hz)');

    Here results:

    ADXL354 datasheet reports gain 0,5 (@1500 Hz) due to low-pass internal filter.

    Green stars are reference points from ADXL354 datasheet frequency response (fig. 7).

    Due to low-pass filter, frequency response should be 0.5 instead 1.09 (first green star), so I suppose blue line would be "core" response, but in this case value at 1500 Hz should be in red cross.
    Regardless Q value of second order system response (wao is given in datasheet) I can't reach red cross value...

    If I apply a second order low-pass filter (yellow line) output response (violet line) fits better, but not exactly as datasheet plot so I suppose it isn't correct model.

    So, is there any way to model core accelerometer and analog (is it really an analog sinc filter? It feels strange datasheet would be wrong but I've never noticed "analog" sinc filters...) filter?

    About ADXL355, low-pass filter (at 4kHz ODR) is reported as 1000 Hz.... but in this case it's assumed corner value -6dB (0.5) instead -3dB (0.7), right?

    Thanks, Michele.

Reply
  • Goodmorning Anthony, thanks for answer but keep in mind this for my purposes:
    I'm aware seismic instruments (sensors and dataloggers) work at low frequencies with much less noise, but my target is design a cost-effective (compared to professional instruments such as Nanometrics, Kinemetrics, Quanterra, Sara and so on) device.

    Obviously with "lower" performances

    Of course I can buy professional accelerometer for seismic application with no noise, but it works at low frequencies, or  I can buy narrow band accelerometer, with higher cost and high noise.

    My purpose is to compare professional seismic accelerometers (such Titan and Episensor) and MEMS based seismic accelerometers (GeoSig) with commercial MEMS (in sensor arrays such Suricat or stand-alone such Raspberry shields).

    I can get PGA (peak gain acceleration) values during an earthquake from several 4$ MEMS (180ug/sqrt(Hz)), but it would be better if I find for same price (35$ in this aapplication for me stands for "more or less") a 50ug/sqrt(Hz) so I can detect smaller events.

    At same time, I can use MEMS accelerometer for monitor earthquake effects on a building, installing one device for every floor. Which is the difference between a "cheap" LIS344ALH (just for example, to take a "concurrent" sensor) and an ADXL354 (with lower noise)?

    How much will noise affects results on monitoring building?
    How far are results obtained from a professional accelerometer (Titan SMA) and a MEMS based device?
    Could I use a MEMS based device instead professional one? If so, keep in mind for the same price of Titan SMA I can fill a building with at least 10-15 devices or, for same budget, monitor 10-15 buildings instead only one.

    So you can understand comparing "on the fly" professional instruments and cost-effective deevices is not so easy just reading sensor datasheet.
    Then you can see comparing different sensors on shake-table will give you different results in terms of phase delay (and so in terms of waves analysis) even if transfert function (magnitude) is more or less the same (that's why researchers who will perform analysis asks me poles/zeros and/or filter coefficients).

    Ok, let's come back to ADXL: ADXL354 is perfect for our characteristics in terms of selectable range, frequency range (0-1000Hz), cost and self noise.
    I selected this MEMS also because same "core" is available in both analog and digital version.

    As you correctly said in your answer I can add an external ADC for ADXL354, but this means I can increase space and components number: between LIS344ALH (I use this as example because I've already seen it in seismic devices) with external signal conditioning and ADC, and ADXL355, which do you think I'll prefer if I need to design a board for Intel Edison?

    I understand you can't tell me factory "secrets" of ADXL sensors, but for my purpose just "take a look to datasheet plots" doesn't help me so much.

    For ADXL001 (I've found a thread in this forum) it's reported on datasheet both resonant frequency and quality factor, so there was a Matlab script for modeling accelerometer core.

    I used same script with no success.

    s=tf('s');
    wao=2*pi*2400;
    qao= 10;
    qao= 11*1.276;

    NUMa=wao^2;
    DENa=[1 wao/qao wao^2];
    Ha=tf(NUMa,DENa);

    freq(1:5000)=1:5000;
    omega(1:5000)=2*pi*freq(1:5000);
    [ma,pa]=bode(Ha,omega);
    Ma(1:5000)=(abs(ma(1,1:5000)));


    % reference from ADXL354 graph
    x_ref=[1500,2132, 2400,2795, 3000, 4000, 5000];
    y_ref=[1.09,2, 6.7, 2,1, 0.2, 0.1];


    loglog(freq,Ma,'-b',x_ref,y_ref,'g*', 1500, 2*1.09, 'rx');

    grid on;
    hold on
    ylim([0.01 10]);
    xlim([10 5000]);
    ylabel('Xout [g]');
    xlabel('FREQUENCY [Hz]');
    title('ADXL354 frequency response for X-Axis');
    legend('hypothetical accelerometer core (Wr=2.4kHz, Q=11)', 'ADXL354 datasheet', 'core value (@1500 Hz)');

    Here results:

    ADXL354 datasheet reports gain 0,5 (@1500 Hz) due to low-pass internal filter.

    Green stars are reference points from ADXL354 datasheet frequency response (fig. 7).

    Due to low-pass filter, frequency response should be 0.5 instead 1.09 (first green star), so I suppose blue line would be "core" response, but in this case value at 1500 Hz should be in red cross.
    Regardless Q value of second order system response (wao is given in datasheet) I can't reach red cross value...

    If I apply a second order low-pass filter (yellow line) output response (violet line) fits better, but not exactly as datasheet plot so I suppose it isn't correct model.

    So, is there any way to model core accelerometer and analog (is it really an analog sinc filter? It feels strange datasheet would be wrong but I've never noticed "analog" sinc filters...) filter?

    About ADXL355, low-pass filter (at 4kHz ODR) is reported as 1000 Hz.... but in this case it's assumed corner value -6dB (0.5) instead -3dB (0.7), right?

    Thanks, Michele.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.