Post Go back to editing

ADXL372 external synchronization

Hello

Our customer will use ADXL372 at external sync (2000Hz) and internal clock (ODR=3200 Hz setting).

Datasheet rev.0 P24  "SYNCHRONIZED DATA SAMPLING" says below.

"

The EXT_SYNC is an active high signal. Due to the asynchronous
nature of the internal clock and external sync, there may be a
one ODR clock cycle difference between consecutive external sync
pulses. "

Question

What does one ODR clock cycle difference  mean ?

I think  that  ADXL372  outputs date at 1/3200 second after sync (every 1/2000 second )

when SYNC is 2000Hz and ODR setting is3200Hz (internal clock ).

Please let me know your advice how  "one ODR clock cycle difference" affects ADXL372 operation .

Regards,

Terumasa

Parents
  • Hello -san, 

    For your question:

    1:

    Which  is the sample timing of internal ADC  based on  the EXT_SYNC or  internal clock?

     

    Answer: The sampling of the internal ADC depends on the user selected ODR. Since you chose to use an EXT_SYNC signal, which then sets the ODR, the ADC sampling rate is now equal to the EXT_SYNC signal's frequency.

     

    2

    The relationship of the internal clock and external sync are asynchronou.

    Is the acceleration data of ADXL372 interpolated 

    as the sample timing of accleration data  equals the timing trrigered by EXT_SYNC?

     

     

    Answer: As far as the datasheet is concerned, there is no mentioning of an interpolation of the acceleration data. 

     

    3

    Does below timing chart  describes  Data ready ?

     

     

    If this is data ready,  this timing chart means that one data is lost.

    Could you teach me why the data is lost ?

    If there is the timing chart which indicates this reason, could you provide me of it ?

     

    Answer: In the case of using an EXT_SYNC signal, the acceleration samples are produced every time the EXT_SYNC signal goes high. This means that it also sets the DATA_RDY bit every time a new valid data is available. Yes, that would mean that data for one cycle would be lost but still this may only happen as stated in the data sheet which means that it is only a possibility and may not happen at all times. This happens due to the asynchronous nature of the internal clock and external sync.

    As the sample statement on the data sheet says "For example, if sending an external sync at a 2 kHz rate, all 3 axes (if enabled) are sampled in that 2 kHz window", with your customer's application using the same frequency of 2 kHz, this means that the acceleration data is sampled in the 2 kHz window. 

     

    I hope that this has helped answer your questions.

     

    Regards, 

    JP

Reply
  • Hello -san, 

    For your question:

    1:

    Which  is the sample timing of internal ADC  based on  the EXT_SYNC or  internal clock?

     

    Answer: The sampling of the internal ADC depends on the user selected ODR. Since you chose to use an EXT_SYNC signal, which then sets the ODR, the ADC sampling rate is now equal to the EXT_SYNC signal's frequency.

     

    2

    The relationship of the internal clock and external sync are asynchronou.

    Is the acceleration data of ADXL372 interpolated 

    as the sample timing of accleration data  equals the timing trrigered by EXT_SYNC?

     

     

    Answer: As far as the datasheet is concerned, there is no mentioning of an interpolation of the acceleration data. 

     

    3

    Does below timing chart  describes  Data ready ?

     

     

    If this is data ready,  this timing chart means that one data is lost.

    Could you teach me why the data is lost ?

    If there is the timing chart which indicates this reason, could you provide me of it ?

     

    Answer: In the case of using an EXT_SYNC signal, the acceleration samples are produced every time the EXT_SYNC signal goes high. This means that it also sets the DATA_RDY bit every time a new valid data is available. Yes, that would mean that data for one cycle would be lost but still this may only happen as stated in the data sheet which means that it is only a possibility and may not happen at all times. This happens due to the asynchronous nature of the internal clock and external sync.

    As the sample statement on the data sheet says "For example, if sending an external sync at a 2 kHz rate, all 3 axes (if enabled) are sampled in that 2 kHz window", with your customer's application using the same frequency of 2 kHz, this means that the acceleration data is sampled in the 2 kHz window. 

     

    I hope that this has helped answer your questions.

     

    Regards, 

    JP

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.