Post Go back to editing

ADIS16223 Rev0 Data sheet typos?

Are these typos? The Rev 0 Data sheet for ADIS16223 as downloaded from AD website has a couple of important typos.

Page 14 of 20

Alarm Indicator states "Set GLOB_CMD[4]=1 (DIN = 0xBF10)"

The DIN should be 0xBE10 not 0xBF10 ?

 

Page 15 of 20

Self-Test states "Set GLOB_CMD[2] = 1 (DIN = 0xBE02)"

The DIN should be 0xBE04 not 0xBE02 ?

 

I have drawn up a table based on Table 27 but with the addition of the DIN commands as I understand them.

Please can you check the above observations and the table below for accuracy / errors.

Are the observations above due to typos or have I misunderstood the GLOB_CMD[x] commands?

Bits Din command Description
15 0xBF80 Reserved
14 0xBF40 Reserved
13 0xBF20

Restore capture data and settings

12 0xBF10

from flash memory

11 0xBF08

to flash memory

10 0xBF04 Set CAPT_PNTR = 0x0000
9 0xBF02 Reserved
8 0xBF01 Clear capture buffers
7 0xBE80 Software reset
6 0xBE40 Reserved
5 0xBE20

Flash test, compare sum of flash

4 0xBE10

memory with factory value

3 0xBE08

Restore factory register settings

2 0xBE04

and clear the capture buffers

1 0xBE02 Power-down
0 0xBE01 Autonull
Parents
  • Can you re-check BE02 / BE04 GLOB commands.

    Logic based on bit positions as published in table 27 would make

    Self-Test states "Set GLOB_CMD[2] = 1 (DIN = 0xBE04)

    But I and others use 0xBE02 for self test. Could the error be the bit position stated in Table 27, rather than the DIN?

    So it could say Self-Test states "Set GLOB_CMD[1] = 1 (DIN = 0xBE02)"

    This would mean it clashes with bit position for Power-down so that would need to be looked at too.

Reply
  • Can you re-check BE02 / BE04 GLOB commands.

    Logic based on bit positions as published in table 27 would make

    Self-Test states "Set GLOB_CMD[2] = 1 (DIN = 0xBE04)

    But I and others use 0xBE02 for self test. Could the error be the bit position stated in Table 27, rather than the DIN?

    So it could say Self-Test states "Set GLOB_CMD[1] = 1 (DIN = 0xBE02)"

    This would mean it clashes with bit position for Power-down so that would need to be looked at too.

Children
No Data