Are these typos? The Rev 0 Data sheet for ADIS16223 as downloaded from AD website has a couple of important typos.
Page 14 of 20
Alarm Indicator states "Set GLOB_CMD[4]=1 (DIN = 0xBF10)"
The DIN should be 0xBE10 not 0xBF10 ?
Page 15 of 20
Self-Test states "Set GLOB_CMD[2] = 1 (DIN = 0xBE02)"
The DIN should be 0xBE04 not 0xBE02 ?
I have drawn up a table based on Table 27 but with the addition of the DIN commands as I understand them.
Please can you check the above observations and the table below for accuracy / errors.
Are the observations above due to typos or have I misunderstood the GLOB_CMD[x] commands?
Bits | Din command | Description |
15 | 0xBF80 | Reserved |
14 | 0xBF40 | Reserved |
13 | 0xBF20 | Restore capture data and settings |
12 | 0xBF10 | from flash memory |
11 | 0xBF08 | to flash memory |
10 | 0xBF04 | Set CAPT_PNTR = 0x0000 |
9 | 0xBF02 | Reserved |
8 | 0xBF01 | Clear capture buffers |
7 | 0xBE80 | Software reset |
6 | 0xBE40 | Reserved |
5 | 0xBE20 | Flash test, compare sum of flash |
4 | 0xBE10 | memory with factory value |
3 | 0xBE08 | Restore factory register settings |
2 | 0xBE04 | and clear the capture buffers |
1 | 0xBE02 | Power-down |
0 | 0xBE01 | Autonull |