Post Go back to editing

ADIS16375 output noise

Thread Summary

The user asked how to calculate the noise variance of the Gyro and Accelerometer outputs for the ADIS16375, given a 2kHz Sync clock input and DEC_RATE set to 100 (decimal). The final answer provided the formula: Noise = noise-density x sqrt(1.57 x ODR/2), where ODR = 2000/(100 + 1) = 19.8 SPS. For the gyroscope, the noise is 0.08 deg/sec (rms), and for the accelerometer, it is 0.36 mg (rms).
AI Generated Content

Hi, everybody!

Here is my question:

With my ADIS16375, I use DIO1 as a 2kHz Sync clock input, DEC_RATE set as 100, so how can I calculate the noise variance of Gyro and Accelerometer output according to the datasheet? How to use parameters like "Output Noise", ''Rate Noise Density", etc?

I'm just new to these, thanks for your patient reply!