Post Go back to editing

Difference between ADXL325 and ADXL326 X axis Y axis Z axis sensor

My customers are checking the performance difference of the three axis sensors for design the accelerometer.
Is the same performance for the ADXL325 and ADXL326 three axis sensors on the X, Y, Z axis?
Assume that each axis is set to the same bandwidth.
In the data sheet, I seem to have no performance difference on the three axes.
If different, is there a document showing the difference about each axis?
Best regards
Parents
  • I'm sorry
    I arranged the question.

    In the ADXL 326 datasheet, the X, Y and Z axes have the same noise density (300 μg / √Hz rms).
    The X and Y axes are BW 1600 Hz and the Z axis is 550 Hz.

    If the same filter (eg 500 Hz: 0.01 μF) is set for all axes
    The X, Y and Z axes have the same noise floor.
    Is this correct?

     

    Best regards
Reply
  • I'm sorry
    I arranged the question.

    In the ADXL 326 datasheet, the X, Y and Z axes have the same noise density (300 μg / √Hz rms).
    The X and Y axes are BW 1600 Hz and the Z axis is 550 Hz.

    If the same filter (eg 500 Hz: 0.01 μF) is set for all axes
    The X, Y and Z axes have the same noise floor.
    Is this correct?

     

    Best regards
Children
No Data