Post Go back to editing

Difference between ADXL325 and ADXL326 X axis Y axis Z axis sensor

Thread Summary

The user inquired about the performance differences between the X, Y, and Z axes of the ADXL325 and ADXL326 three-axis sensors. The final answer clarified that while the performance of each axis is consistent regardless of orientation, it is not guaranteed to be exactly the same across all axes. The datasheet specifies different bandwidths for the Z axis (550 Hz) compared to the X and Y axes (1600 Hz), but the noise density is the same (300 μg/√Hz) for all axes. Setting the same filter (e.g., 500 Hz) for all axes will result in the same noise floor for each axis.
AI Generated Content
My customers are checking the performance difference of the three axis sensors for design the accelerometer.
Is the same performance for the ADXL325 and ADXL326 three axis sensors on the X, Y, Z axis?
Assume that each axis is set to the same bandwidth.
In the data sheet, I seem to have no performance difference on the three axes.
If different, is there a document showing the difference about each axis?
Best regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.