We use these accelerometers well above their 125C rating. They are relatively inexpensive and have the range we need. What is the replacement for these when they are gone?
ADXL193
Obsolete
The ADXL193 is a small (5 mm x 5 mm x 2 mm ceramic LCC package), low power (1.5 mA current at 5V), single axis high-g iMEMS® accelerometer designed to...
ADXL193 on Analog.com
ADXL278
Obsolete
The ADXL278 is a low power, complete, dual-axis accelerometer with signal conditioned voltage outputs that are on a single monolithic IC. This product...
ADXL278 on Analog.com
We use these accelerometers well above their 125C rating. They are relatively inexpensive and have the range we need. What is the replacement for these when they are gone?
Thank you for using these products in your work and for your post! Unfortunately, we do not have direct replacements for these devices but are releasing a number of accelerometers that might be worth your consideration. To start with, you might want to consider the ADXL1001 or ADXL356.
http://www.analog.com/en/products/mems/accelerometers/adxl1001.html
http://www.analog.com/en/products/mems/accelerometers/adxl356.html