Post Go back to editing

Difference between ADXRS450, ADXRS810, and ADXRS453?

Thread Summary

The user inquires about the differences between the ADXRS450, ADXRS810, and ADXRS453 gyroscopes, particularly in their function and testing. The final answer indicates that the ADXRS453 includes temperature-dependent calibration, while the ADXRS450 does not. The ADXRS810, designed for automotive use, shares a similar core sensor but is not supported in this forum. The high-vibration version (ADXRS453) has a 1°/sec/g drift, compared to 3°/sec/g for the other two models.
AI Generated Content

I am looking for a very accurate gyro for a robotics application and came across the ADXRS450, ADXRS810, and ADXRS453. They all appear to have the same specifications, but are rated for medical, automotive, and high vibration settings. What are the differences in the actual function (if any)? Are the more expensive medical and high-vibration versions simply better tested? The high-vibration version seems to have 1*/sec/g drift compared to 3*/sec/g for the other two, but is that the only difference?

  • As of right now, we don't provide support for automotive parts in this forum (ADXRS810), but from what I understand, it does use a similar core sensor as the ADXRS450 and ADXRS453.  The ADXRS453 includes some calibration for temperature dependent behaviors, while the ADXRS450 does not.  They do use much of the same core sensor design, but I do believe that there are subtle differences in their final configuration.  What type of application is this for?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.