Post Go back to editing

ADXL355 Sampling Frequency

Thread Summary

The user inquired about the ADXL355's sampling frequency error and jitter. The final answer indicated a clock variation of approximately 3.5%, suggesting an external clock for higher accuracy. The accompanying answers discussed external synchronization and interpolation, noting that the SYNC signal is fixed at the sample point and that using an external clock frequency lower than the ODR (e.g., EXT_CLK=200Hz, ODR=250Hz) is not recommended.
AI Generated Content

Hi

I have a question ADXL355 Sampling frequency.

(1) When the sampling frequency was established by 250Hz or 125Hz.
  How much is an error of sampling (250 Hz ± ○○Hz)?


(2) How much is a jitter of sampling?
Even not the specification value, but the force value is good, so please tell me.

If you know ,please tell me...

Best regards

HOD

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.