Hello
I am testing ADXL103. I use three ADXL103 (X , Y, Z) to test.
Experiment:
1. test 0 bias in room temperature;
2.increase 10 Celsius degrees,keep the temperature for 30 minutes,then test 0 bias;
3.Repeat the 2 operation,until the temperature achieving 70 Celsius degrees。
In the Experiment,In the 40 Celsius degrees temperature, the 3 ADXL103 are placed on a plat place without shocking,
The output of Z is not stable,the jump range is 10 mg for long time, then power down and up again,it is not work; shock
Z,it become stable. X , Y both are stable( jump range 1 mg).
In the 64 Celsius degrees temperature, the 3 ADXL103 are placed on a plat place without shocking,
The output of X is not stable,the jump range is 6 mg for long time, then power down and up again,it is not work; shock
X,it become stable. Y, Z both are stable ( jump range 1 mg).
How to solve these problems ,by the way ,my ADXL103 is purchased in 2011.
thank you!