ADXL343
Recommended for New Designs
The ADXL343 is a versatile 3-axis, digital-output, low g MEMS accelerometer. Selectable measurement range and bandwidth, and configurable, built-in motion...
Datasheet
ADXL343 on Analog.com
ADXL345
Production
The ADXL345 is a small, thin, low power, 3-axis accelerometer with high resolution (13-bit) measurement at up to ±16g. Digital output data is formatted...
Datasheet
ADXL345 on Analog.com
Hi
what kind of differences are between ADXL343 and ADXL345,
except samplerates below 6.25Hz for ADXL343?
In Selection Table (the link is here: Selection Table for MEMS Accelerometers )
Bandwidth -3dB for ADXL345 is 1.6kHz and only 0.32kHz for ADXL343
But it seems 0.32kHz for ADXL343 to be mistake,
cause in the Datatsheet the highest samplerate for ADXL343 is 3200Hz and appropriate bandwidth 1600Hz
Hi bnv123
These two are quite similar. The main differences between the ADXL343 and ADXL345 are related to the minimum and maximum specifications, which are provided for the ADXL345 but not mentioned for the ADXL343.
Regards,
Mohammad
Hi bnv123
These two are quite similar. The main differences between the ADXL343 and ADXL345 are related to the minimum and maximum specifications, which are provided for the ADXL345 but not mentioned for the ADXL343.
Regards,
Mohammad