Post Go back to editing

ADXRS645 mounting location

Thread Summary

The user inquired about mounting the ADXRS645 gyro off the axis center line due to a central bore with fluid flow. The final answer confirmed that the gyro will measure the rate of rotation accurately regardless of its position relative to the axis, eliminating the need for calibration based on distance from the center.
AI Generated Content

The new ADXRS645 gyro looks like it could suit our requirements for but we have restrictions on where we can mount the device, a central bore with fluid flow will not allow us to locate it so that the rate axis rotation will be dead centre. Can the gyro be mounted off the axis centre line (approx. 3cm) and if so how do I calibrate the output according to the distance from centre?

Parents Reply Children
No Data