On the "Not Recommended for New Designs" ADXL321 page ADXL326 is indicated as a replacement part. But for the ADXL326 supply voltage range is 1.8 to 3.6V while for the ADXL321 supply voltage range is 2.4 V to 6V. So ADXL326 is not a suitable replacement for the ADXL321 for the 5V supplied systems.
Does the 5V supplied pin-to-pin compatable replacement for the ADXL321 exist and what is the possible production period for this part?
Also I have noticed the ADXL203 is not recommended for new designs too.
Is it applied for all versions (ADXL203, AD22037 and AD22293) or only for 1.7g version?
What is a replacement for the AD22037 and AD22293?
Regards,
Roman