ADXL001
Obsolete
The ADXL001 is a major advance over previous generations of accelerometers providing high performance and wide bandwidth. This part is ideal for industrial...
ADXL001 on Analog.com
ADXL180
Not Recommended for New Designs
The ADXL180 iMEMS® accelerometer is a configurable, single
axis, integrated satellite sensor that enables low cost solutions
for front and side impact...
Datasheet
ADXL180 on Analog.com
Hi,
I've been working on vibration monitoring project that must have ~200g range and extended temp of up to 150 degC.
I did a preliminary search on ADI's MEMS product line, and it seemed only ADXL001 and ADXL180 were suitable.
I would prefer to implement a 3-axis, digital output accels if you have such product.
Thanks
Hi Robin,
The closest product we could offer would be the ADXL375 but it is rated only to 85C. You can probably stretch it to ~105C if you are not too concerned about DC performance.
Regards,
Venkat