Post Go back to editing

ADIS16209 assembly issue

Thread Summary

The user is experiencing issues with ADIS16209 sensor boards, where seven out of eight boards in Set A failed after hand-soldering a 1.27mm connector, while all boards in Set B worked. The final answer suggests probing key SPI signals to compare working and non-working boards and mentions the availability of a failure analysis service. The user is also advised to check the PROD_ID register (DIN = 0x4A00) for communication differences.
AI Generated Content

Hi,

          We have designed some sensor board based on ADIS16209 and are having some assembly issue. We had two sets of PCBs (set A - 8 PCBs and Set B - 10 PCBs) with automated machine mounting of this IC. Only components to be soldered manually were 1.27mm connector that we did inhouse. In set A of the PCBs, seven boards out of eight boards failed (IC did not get recognized in software) while in the other set, all of the 10 PCBs were working. As far as I remember I did not apply excess heating in soldering (I had set 280 deg. C in my weller soldering station, WSD 81i with 0.2mm soldering tip) 1.27mm connector for set A while other set of PCBs were soldered with some other soldering station with 2mm tip and set at 315 deg. C. I am still puzzled with the IC sensitivity whether it could be failed due to soldering some nearby components.

Is there any way to identify whether IC is still functional or gone dead. I am hooking SPI analyser but it does not show any communication on MISO line.

Regards,

Varindra

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.