Post Go back to editing

ADXRS652 Power Supply Design and Noise Density

Thread Summary

The user inquired about the ADXRS652 gyroscope's noise and ADC resolution requirements. For a 2.5kHz bandwidth, the noise is calculated as 3°/s, which is greater than the 16-bit ADC's resolution of 0.0127°/s. A 12-bit ADC is suggested as sufficient for maintaining in-run bias stability. For high precision, the Vdd can be powered by an LDO, Vratio by a high-precision 5V reference, and AVcc can be tied to Vdd with proper decoupling.
AI Generated Content

We use ADXRS652 in our new products and noticed the Rate Noise Density of this gyro is 0.06°/s/√Hz,  does it means if the bandwidth is 2500Hz, the noise is 0.06*√2500=3°/s?

We are going to use a 16bit A/D to convert gyro's output to digital, the resolution should be 0.0127°/s, if the gyro's bandwidth is 2.5KHz, the noise is 3°/s and greater than A/D resolutioin, in that case, seems a 10bit A/D is enough, am I right?

Since the noise density is 0.06°/s/√Hz, a 16bit A/D will enough to whole bandwidth application, is it correct?

Anohter quesition is about the power supply of the ADXRS652, there is 3 power supply pins, Vdd, AVcc and Vratio, based on my understanding, all  power supply pins can be connect to a single supply if high precision is not needed. If high precision is needed,  3 power supplys used to Vdd, AVcc and Vratio separately may be is the best option, but 3 power supply may cost more.

In our case (high precision and high bandwidth needed), we are going to use a LDO (1% precision) for the Vdd, use a high precision 5V reference for the Vratio, but what should we do about the AVcc? If we use LDO to power supply AVcc, may be the precision in not enough, but if we use the 5V reference to the AVcc, may be the 5V reference supply current is not enough cause 3 gyro used on one pcb board.

Is there any applicaion notes about ADXRS652 power supply design or spcefictaion of the AVcc operating current and precision?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.