Post Go back to editing

How precise is the Dualaxis AD22302 accelerometer?

Hello everyone


I am a mechanical engineering student currently working on a project,

wich involves working with an AD22302 Dual-Axis accelerometer.

It is capable of measuring +/- 70g on the x-axis wich is the one I am currently using.


My question is:

what is the accuracy of the device? I am able to find the non-linearity in the datasheet (attached to the post)

but that is about it and I need the overall accuracy. Any kind of help will be highly appreciated


- Jesper

Accelerometre_AD22300_1_2.pdf
Parents
  • Hi Mark,

    Last week I made a couple of tests were the difference between expected output and the measured input was 5-20 % off but in the mean time I found that a lot of noise were coming from vibrations from the device itself after it had been hit. And the method of wich I were obtaining expected input acceleration were too inaccurate. So I will start testing again tomorrow and see how much it helped, hopefully I will stay under a 10 % difference in expected and measured acceleration.

Reply
  • Hi Mark,

    Last week I made a couple of tests were the difference between expected output and the measured input was 5-20 % off but in the mean time I found that a lot of noise were coming from vibrations from the device itself after it had been hit. And the method of wich I were obtaining expected input acceleration were too inaccurate. So I will start testing again tomorrow and see how much it helped, hopefully I will stay under a 10 % difference in expected and measured acceleration.

Children
No Data