Post Go back to editing

How to declare and use the SPI ADIS16209 sensor with the IIO driver?

We are using the ADIS16209/PCBZ in a Beaglebone Black system running Ubuntu 13.04, using the SPI interface.


We have done a preliminary test using the Adafruit Python libraries and the sensor was working. But for our application we need to use the IIO Linux driver available in the following page:

https://wiki.analog.com/resources/tools-software/linux-drivers/iio-accelerometer/adis16209?rev=1353005312


Every documentation that we have read so far refers that "Each and every IIO device, ... has a device folder under /sys/bus/iio/devices/iio:deviceX."


Our problem is that we don't have such device folder in our system. We suppose that some additional instruction is required to say that a IIO device is connected to SPI0, but couldn't figure out what. I guess our problem is with declaring the SPI slave devices. I realize that we should run __init board_init() according to the instructions on the above mentioned IIO driver web page, but I don't know where and how I should run that code.


If it is available please recommend some web page where I can find code snippets for reading from the sensor with IIO.


I give some more details below that may be of interest for understanding our issue.


 

ADDITIONAL INFO:


1) connection of the iSensor ADIS16209 (port SPI0 of Beaglebone Black, /dev/spidev1.0)

 

ADIS conector J1
BBB P9
2 (SCLK)
22 (spi0_clk)
3 (/CS)
17 (spi0_cs0)
4 (DOUT)
21 (spi0_d0)
6 (DIN)
18 (spi0_d1)
10, 11 or 12 (VDD)
3 ou 4 (DC_3.3V)
7 or 8 (GND)
1 ou 2 (GND)


2) to manually load the device tree overlay

# cat /lib/firmware/BB-SPIDEV0-00A0.dtbo > /sys/devices/bone_capemgr.9/slots

result: the devices /dev/spidev1.0 and /dev/spidev1.1 are automatically created.


To install in the boot, the following line was added to "/boot/uboot/uEnv.txt":

optargs=capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN capemgr.enable_partno=BB-SPIDEV0


The first part deactivates HDMI, and the second loads the device tree overlay.


3) The content of /etc/modules is as follows:


# /etc/modules: kernel modules to load at boot time.
# This file contains the names of kernel modules that should be loaded
# at boot time, one per line. Lines beginning with "#" are ignored.
# Parameters can be specified after the module name.
iio_hwmon
ring_sw
adis_lib
adis16209


Parents
  • Hello Lars,

    I want to thank you for the valuable tip. I was stuck on that for quite some time.

    Could you give some advice on the best way to use the driver from a C++ program? There are any guides or example source code online for me to get started? Should I use the iioutils libray?

    Thanks again for your support.

    Very best,

    Rafa

Reply
  • Hello Lars,

    I want to thank you for the valuable tip. I was stuck on that for quite some time.

    Could you give some advice on the best way to use the driver from a C++ program? There are any guides or example source code online for me to get started? Should I use the iioutils libray?

    Thanks again for your support.

    Very best,

    Rafa

Children
No Data