Post Go back to editing

Noise peformance on ADXL345 and ADXL202

I wondered which has a better noise peformance between analogoutput type and digital outputtype.
According to the datasheet ADXL202(analog output type),
The output noise is 1.4mg_rms@100Hz from Table 7.
http://www.analog.com/static/imported-files/data_sheets/ADXL103_203.pdf

On the other hand, ditital output type, ADXL345's noise peformance is 0.75LSBrms LSB@100Hz from the datasheet.
http://www.analog.com/jp/mems-sensors/mems-inertial-sensors/adxl345/products/product.html

I'm not sure that which is a better spec between 0.75LSBrms and 1.4mg_rms.
Please tell me how to compare [mgrms] and [LSBrms].

Best,
Tarzan

Hi Tarzan,

The sensivity of ADXL345 is 3.9mg/LSB, so 0.75LSBrms meanse 0.75 * 3.9 = 2.925mg_rms. It is worse than 1.4mg_rms. What's more, ADXL202 is obsolete, ADXL203 is recommended to replace it.

BR

Neil

  • Hi Neil,

    Thanks for your prompt reply.

    I understand it.

    Best regards,

    Tarzan

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin