Post Go back to editing

Problems with ADIS16265 EVAL Board ...

Thread Summary

The user experienced inconsistent voltage readings and low power diagnosis from an ADIS16265 Gyro evaluation board, with values fluctuating between 1.9V and 4.9V. The issue was resolved by replacing the evaluation board, suggesting a potential cold soldering problem. The new board provided stable readings and correct voltage values immediately upon connection.
AI Generated Content

Hi everybody,

I am just working on the implementation of a ADIS16265 Gyro into my roboter application and a have problems

with the readings of the Evaluation board.

The Board is sending sometimes stupid values.

i.e: I am asking for the voltage of the board and get  values between 1.9 ... 4.9 Voltage back.

Sometime, the board is sending for a long time the correct value, which is around 4.95 Voltage,

Which I check with a oscilloscope. The ripple is around 5mV, which should be o.k. as well.

The diagnosis status is saying as well, that it is low power on the chip (sometimes).

It is a LGA mounted chip and I can only check the voltage up the connector of the board, which is fine.

Not on the controller directly.

Does somebody has bad experience with this chip as well ?

Or can this behaviour happen by a software failure. Communication to a other SPI Client is running well.

Is the a test program existing for a atmega - controller, where I can check, if it is a software or Hardware failure.

Best regards

R.

Parents
    1. What is the attached picture showing us? I can't see the transitions and wonder if we are losing important information (noise, ringing, etc)
    2. You do not need to run 5V on your logic. 
    3. If the DOUT is moving to +5V, it is because the ADIS16265 has put it in a tri-state (very high output impedance) and it is floating there due to external influences.
    4. You do not need C1 or C2 in place.
Reply
    1. What is the attached picture showing us? I can't see the transitions and wonder if we are losing important information (noise, ringing, etc)
    2. You do not need to run 5V on your logic. 
    3. If the DOUT is moving to +5V, it is because the ADIS16265 has put it in a tri-state (very high output impedance) and it is floating there due to external influences.
    4. You do not need C1 or C2 in place.
Children
No Data