Post Go back to editing

ADXL78 output - RC

Thread Summary

The user inquired about the need for an external RC filter for the ADXL78, given the Capacitive Load Drive (1000pF) specified in the datasheet. The support engineer confirmed that the internal Bessel filter does not require an external RC filter, and only recommends RC for power supply decoupling as detailed in the Applications section of the datasheet. The output capacitance of the ADXL78 is not specified, but the user was directed to the ADXL001 for reference.
AI Generated Content

Hi,

there isn't any information about an external RC-filter in the datasheet for ADXL78 but only Capacitive Load Drive (1000pF) in the Specification table is shown.

Should one place external RC-filter (or only  C) and what about R,C values?

Or may be internal Bessel filter doesn't require external RC filter?

Is the output capacity of the ADXL78 the same as for the ADXL001? (There was already post about the ADXL001 output here)