Post Go back to editing

Register setting for ADXL343 without use of MCU?

Thread Summary

The user inquires about using the ADXL343's double tap function to trigger an audio playback chip without a processing unit. The final answer confirms that the ADXL343 requires initialization and cannot be pre-configured. An accompanying answer suggests using a small PIC microcontroller, such as the PIC10LF322, to initialize the ADXL343.
AI Generated Content

Good Monday,

I'm specifying an ADXL343 as a component in a very small, inexpensive consumer electronics device that has no processing unit capability. I would like to use the double tap function to trigger an audio playback chip by pulling the int pin low on double tap. I didn't see any documentation in the datasheet talking about hardcoding registers and wonder how one does this or if it is possible to modify / store register settings on the chip even during power off.

Cost is the primary driver for not having a MCU on the board.

Thanks for your help.

J

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.