Post Go back to editing

A simple gyroscope scale factor test using IMU Evaluation

Thread Summary

The user asked about testing the gyroscope's scale factor in the ADIS16485 using IMU Evaluation software. The solution involves setting DEC_RATE to 0x003D, NULL_CFG to 0x070A, and GLOB_CMD to 0x0001, then capturing 500 un-scaled Z_GYRO samples. By integrating the gyroscope data points over time, the angle can be estimated, showing 180 degrees of angular displacement and returning to zero.
AI Generated Content

Is there a simple way to test the gyroscope's scale factor in the ADIS16485, using the IMU Evaluation software?

  • Yes!  The following exercise leverages techniques for observing gyroscope sensitivity (scale factor), which are described in this post (and links provided in this post).

    https://ez.analog.com/message/44891#44891

    1. Start with establishing a known "turn angle." I have found that using a fixed object, as a stop, provides a simple way for turning a gyroscope around a "half-circle," or 180 degrees. See the two pictures below, which show the ADIS16485AMLZ, mounted to an EVAL-ADIS. In this example, the range of motion is limited by the edge of a seminar book, which is pressed up against a cubicle wall in an office. I like simple!

    2. Start the IMU Evaluation software and use it to configure both IMU and the data capture process.  Here is a summary of the settings, which are critical for this exeriment and are reflected in the figures below.

    • DEC_RATE = 0x003D, sets ADIS16485 sample rate to ~39.68 SPS (2460/62)
    • NULL_CFG = 0x070A, sets the average record size to ~26.6 seconds.
    • GLOB_CMD = 0x0001, executes an auto-null for the gyroscopes
    • Total number of samples in the record = 500 samples (~12.5 seconds, total record time)
    • Un-scaled data (no reason for this, other than personal preference)
    • Select Z_GYRO, 32-bit register

    3. Click on Start, then move the ADIS16485/EVAL-ADIS around 180 degrees, then back.  See the embedded video link for example of the motion used in this test.

    4. See the attached Excel file for the data and calculations, but the angle computation is greatly simplified by the sychronous data capture in the EVAL-ADIS.  Simply divide each gyroscope data point by the sample rate, then add them all together to produce a real-time angle estimate. As we can see from the plot, the integrated result shows 180 degrees and angular displacement and the device returns to zero.

    ADIS16485_Scale_Test_Example.xlsx