Post Go back to editing

ADXL206 Zero G Bias Repeatability

Thread Summary

The user inquired about the '0 g bias repeatability' of +/- 10 mg in the ADXL206 spec sheet, specifically if it affects post-calibration accuracy after power cycling. The final answer clarifies that this repeatability value is related to end-of-life drift over 10 years at +25°C, and the degradation model is closer to a square root of time approximation. The accompanying answers suggest that the repeatability value without a time-of-validity component is not very useful and that short-term repeatability may be significantly different.
AI Generated Content

In the ADXL206 spec sheet on page 3, the "0 g bias repeatability" is listed as "+/- 10 mg."  Sorry if this question is obvious, but could someone clearly define what that means?  Is that the turn-on to turn-on repeatability of the sensor?  What I'm curious about is if I temperature calibrate / compensate an ADXL206 at one turn on for scale factor and bias errors, then cycle power on the ADXL206 off and attempt to use my previous temperature compensation, assuming that compensation was perfect will there be a possible additional error of +/- 10mg?  Thanks to anyone who can shed further light on this!