What are the key differences between the ADXRS453 and ADIS16265?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADXRS453
Recommended for New Designs
The ADXRS453 is an angular rate sensor (gyroscope) intended for industrial, instrumentation, and stabilization applications in high vibration environments...
Datasheet
ADXRS453 on Analog.com
ADIS16265
Production
The ADIS16260 and ADIS16265 are programmable digital gyroscopes that combine industry-leading MEMS and signal processing technology in a single compact...
Datasheet
ADIS16265 on Analog.com
What are the key differences between the ADXRS453 and ADIS16265?
The ADIS16265 is a temperature-calibrated gyroscope, in an 11.2mm, 20-pin LGA, that provides noise/stability performance that is similar to the ADXRS62x family. This was the first temperature-calibrated gyroscope in it's performance class and offers customers a simpler path to optimized performance. When it was released, it provided a new option in the engineering trade space: moderate increate in unit cost (compared to ADXRS62x) in exchange for more conenvient interface (SPI vs analog), 10-20x temperature stability improvements, reduced development risk and faster development cycle times. The ADXRS453 also provides a temperature-calibrated gyroscope and leverages a new, quad-mass structure. This new core offered the following advantages, when compared to the ADXRS62x family:

ADXRS453 Packages ADIS16265
It is important to note that the ADIS16265's noise, stability and vibration rejection is adequate for many applications and it offers a point of value in it's bandwidth (330Hz vs 77Hz) and sample rate (2048 SPS vs 477 SPS). The wider bandwidth can be helpful in managing phase delay for feedback control systems and in some cases, the wider sample rate provides additional opportunity for digital filtering of sensor information.
Answered and Closed