How do I configure the ADUC7026 to communicate with the SPI on the ADIS16135?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADIS16135
Last Time Buy
The ADIS16135 iSensor® is a high performance, digital scope sensing system that operates autonomously and requires no user configuration to produce accurate...
Datasheet
ADIS16135 on Analog.com
ADUC7026
Production
The ADuC7019 / ADuC7020 / ADuC7021 / ADuC7022 / ADuC7024 / ADuC7025 / ADuC7026 / ADuC7027 / ADuC7028 / ADuC7029 are fully integrated,
1 MSPS, 12-bit data...
Datasheet
ADUC7026 on Analog.com
ADIS16133
Obsolete
The ADIS16133 iSensor® is a high performance, digital gyro-scope sensing system that operates autonomously and requires no user configuration to produce...
ADIS16133 on Analog.com
ADIS16136
Not Recommended for New Designs
The ADIS16136 iSensor® MEMS Gyroscope is a high performance, digital gyroscope sensing system that operates autonomously and requires no user configuration...
Datasheet
ADIS16136 on Analog.com
How do I configure the ADUC7026 to communicate with the SPI on the ADIS16135?
Embedded processors typically support SPI communications with multi-purpose SPI ports that have some configurable parameters. These parameters could include serial protocol (SPI, I2C, etc), data length, clock polarity, clock phase, bit order, serial clock rate, etc. While it is important to check the sensor's datasheet for product-specifc settings, Table 7 in the ADIS16135 Datasheet (page 8) offers a summary of typical configuration parametes to look for, which are typically found in serial port control registers. Table 7's contents are provide here, for convenience.
Processor Setting |
Description |
Master |
The ADIS16135 operates as a slave. |
SCLK Rate ≤ 2 MHz |
Maximum serial clock rate. |
SPI Mode 3 |
CPOL = 1 (polarity), CPHA = 1 (phase). |
MSB-First Mode |
Bit sequence. |
16-Bit Mode |
Shift register/data length. |
Answered and Closed