Post Go back to editing

Status of 2 bugs - changing default filter settings, writing into registers over SPI interface

Category: Software
Product Number: CN0549
Has Analog devices fixed the following 2 issues with the CN0549 platform?
  • ability to change default filter selection settings;
  • ability to write into the registers over the SPI interface using the DE10-Nano.
I am planning on using the CN0549 to develop a prototype sensor to monitor bearing vibrations. I had tried to use this in 2021 and found a couple of bugs and ended up using a Teensy processor with the ADXL1002 (not the ideal scenario).
I want to try this platform again if the issues have been fixed. Are there any other major issues that are still open on the CN0549 development board?

This is a follow up to a couple of bugs I had found on this platform in late 2021 and was forced to abandon using this platform

Link to my postings from 2021 are here

ez.analog.com/.../unable-to-change-write-filter-settings-in-the-cn0540-setup-using-the-iio-oscilloscope-software

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.