Hello,
As far as I can tell the ADXL343 datasheet specifies that when using Activity mode for interrupts (as well as tap/double tap) that lower output data rates are achieved by decimating a common sampling frequency, and the common frequency is what is actually used to poll for any activity above your set threshold (page 29 of datasheet). Therefore, it's possible for the accelerometer to detect activity that is above the threshold, send an interrupt to another device which then polls the FIFO buffer for the data collected, and that data might not include the high g spike which initiated the Activity interrupt due to the lower data rate. However, the datasheet does not seem to specify anywhere what this common sampling frequency is and for which data rates it applies to.
I am using the ADXL343 at 800 hz currently, and have it set to Activity mode at 1/2 g as the threshold. Yet, often I see data from the field in which none of the samples were above +-1/2 g. From testing it's clear that the other device polls the data fast enough to not lose it before it leaves the 32 sample FIFO buffer, so that's not an issue. I'm worried that it's actually running at something like 1600 hz or 3200 hz and detecting brief acceleration spikes which end up being unlucky enough to fall in-between the gaps of the 800 hz data rate.
Also the datasheet mentioned an "improved tap" mode which I cannot find reference to anywhere else except this one section, at least not by that name.
Relevant part of Datasheet:


Thanks for any help!