Post Go back to editing

ADMT4000 pull resistor value question (multiple devices on single SPI bus)

Thread Summary

The user is developing boards with 3 ADMT4000 sensors each, using a single SPI bus. They are concerned about the 100kΩ pull-down resistor on the SDO pin, as it seems large. The final answer confirms that 100kΩ was used in testing but suggests a 10kΩ resistor would place the device outside its 200μA load current limit. A 33kΩ resistor is proposed for testing to stay within the current limit.
AI Generated Content
Category: Hardware
Product Number: ADMT4000

Hello,

we are developing a set of boards which will use 15 ADMT4000 sensors during power-up to detect absolute position state of the objects left at shutdown.
Each board will have 3 sensors and we plan on using only one SPI bus due to system constraints, chip select pins will select particular device in daisy chain tree.

Documentation for ADMT4000 gives a weird value of pull resistors, it says that SDO must be connected to GND through 100k resistor, but it seems pretty large.

We have at each board 3 devices (3 SDO pins) connected in parallel at all times, so while taking leakage currents into consideration 100k seems to us  pretty large and we would like to use 10k to meet worst case specs in the datasheet.

Is there any hard reason for 100k pulls and can they be smaller? Im attaching the part from schematic that illustrates our setup with SPI pin in parallel, and this 100k bugs us.




Thanks

Edit Notes

title correction
[edited by: lkosanovic at 12:40 PM (GMT -4) on 9 Sep 2026]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.