Post Go back to editing

ADcmXL3021 no respons to register setting to lower SPS

Category: Hardware
Product Number: ADCMXL3021

We have purchased a total of seven ADcmXL3021 sensors over time in different batches.

For our application, we designed an in-house PCB that interfaces the ADcmXL3021 with an ESP32-S3 microcontroller. The same PCB design and the same firmware are used for all sensors.

In our firmware, the RT_CTRL register is configured with the value 0x0080, which according to our understanding should set the device to an output data rate of 20,000 SPS in RTS mode. Also register REC_CTRL is configured with the value 0x1103, which should put the sensor in RTS mode.

However, with two of the seven ADcmXL3021 sensors, we observe a different behavior. When these sensors are connected to the exact same hardware and operated with the exact same firmware, a logic analyzer shows an output data rate of approximately 220,000 SPS instead of 20,000 SPS.

The serial output of the ESP32-S3 give the following information about the two not working ADcmXL3021 sensors: 
PROD_ID=0x0BCD, SERIAL=0x00EC, REV_DAY=0x0326, YEAR_MON=0x1902

The remaining five sensors operate as expected and output data at approximately 20,000 SPS.

Since the hardware and firmware are identical for all tested units, we are wondering whether this behavior could indicate:

  • a device configuration issue that we may have overlooked,
  • a difference in device revision,
  • a calibration or factory-programmed setting,
  • or a possible device defect.

Has any one encountered similar behavior before, or are there any registers or diagnostics that you would recommend checking?

  • Hello  Thanks for posting, I understand your concern and also agree this is not the expected behavior on a first sight. However most of the applications team is out currently so we have really limited bandwidth to handle your case in enough detail. 

    please keep us posted if you have any other finding, we will try to give some resources to this case as soon as posible.

    Thanks for your time,

    Mario SM

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.