Post Go back to editing

0 g Voltage @ Vs=3.3V

Thread Summary

The user asked about the 0 g voltage of the ADXL203 at a 3.3V power supply. The final answer confirmed that the 0 g voltage is ratiometric to Vs, so at 3.3V, it is 1.65V, as expected. The user acknowledged the answer and thanked the support engineer.

View FAQ
AI Generated Content
Category: Datasheet/Specs
Product Number: ADXL203

The ADXL203 power supply Vs is specified from 3 to 6 V.
The 0 g Voltage at Vs=5V is specified to be 2.5 V.
What is the 0 g Voltage at Vs=3.3V? Is it 1.65 V?
Thanks for the attention.
GF

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.