Post Go back to editing

0 g Voltage @ Vs=3.3V

Thread Summary

The user asked about the 0 g voltage of the ADXL203 at a 3.3V power supply. The final answer confirmed that the 0 g voltage is ratiometric to Vs, so at 3.3V, it is 1.65V, as expected. The user acknowledged the answer and thanked the support engineer.

View FAQ
AI Generated Content
Category: Datasheet/Specs
Product Number: ADXL203

The ADXL203 power supply Vs is specified from 3 to 6 V.
The 0 g Voltage at Vs=5V is specified to be 2.5 V.
What is the 0 g Voltage at Vs=3.3V? Is it 1.65 V?
Thanks for the attention.
GF

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.