Post Go back to editing

Constant z axis offset for -1g

Thread Summary

The user observed a 10% offset in the negative z-axis values of two ADXL355 sensors on a custom board, which was not expected. The final answer suggests that this could be due to mechanical stress, non-symmetrical PCB layout, thermal gradients, or part-to-part variability, and recommends calibration at room temperature using the offset trim registers. The user confirmed the offset is consistent across different boards and sensors, and noted a 100 Hz noise peak in steady state, which may be unrelated.
AI Generated Content
Category: Hardware
Product Number: ADXL355

We use two ADXL355 on our custom board, one on top and the other one on the bottom.

In horizontal position, z axis of the top sensor gives +1g (as expected), while z axis of bottom sensor gives ~ -1.1g.

If we turn the board upside down, we get the same with switched roles.

Having an offset of >= 10% in the negative z axis was not what we expected, and we have never experienced this behavior before.

So my question is has anyone experienced similar constant, steady state offsets for nagtive z axis values? 

Parents
  • Hi  ,

    another thing we noticed, during our analysis, which might be completely unrelated, yet worth to add here:

    In steady state, we observe noises peaks for all axes at around 100 Hz and some (sub)-harmonics, for sensor ODR of 500 Hz. 

    This is perfectly repeatable, even for a battery powered device with no connection to the mains.

    Attached is the plot for y axis, only the peak at ~75Hz is an actual disturbance we know of.

    Also, we measured the VSUPPLY. It is way in between the limits, ~3.27 V. Only V1P8ANA/DIG (generated by internal LDO) are a bit of at ~around 1.72V. Still with remain valid with Vpp ~ 120 mV.

    Kind regards

     

Reply
  • Hi  ,

    another thing we noticed, during our analysis, which might be completely unrelated, yet worth to add here:

    In steady state, we observe noises peaks for all axes at around 100 Hz and some (sub)-harmonics, for sensor ODR of 500 Hz. 

    This is perfectly repeatable, even for a battery powered device with no connection to the mains.

    Attached is the plot for y axis, only the peak at ~75Hz is an actual disturbance we know of.

    Also, we measured the VSUPPLY. It is way in between the limits, ~3.27 V. Only V1P8ANA/DIG (generated by internal LDO) are a bit of at ~around 1.72V. Still with remain valid with Vpp ~ 120 mV.

    Kind regards

     

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.