Post Go back to editing

Unclear temperature difference of approx. 2 Kelvin measuring two PT100 RTDs with 2kΩ shared RSense in 2-Wire-Mode using LTM2985

Category: Hardware
Product Number: LTM2985

Hello ADI,

I have trouble reading the values of two PT100 RTDs as cold junctions for two thermocouples. The RTDs have a shared RSense of 2 kΩ and are configured in 2-Wire-Mode. My schematic is very close to figure 12, “Shared 2-Wire RTD Example”, in the LTC2985 Datasheet (Rev. A) on pages 39 and 40. To illustrate my problem, I have copied the two pages and put my values in.

The data I get for the PT100 cold junctions are both approximately 2 Kelvins too high. I reviewed the schematic and the code intensively but found no error so far. Is it possible that this is a regular aberrance? I would expect the measuring system to be much more precise. Isn't it?

Kind regards,
Mario 

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.