Post Go back to editing

The MAX_PEAK register sometimes returns all 3 values ​​as 0

Thread Summary

The user is experiencing issues with the HIGHEST PEAK DATA registers returning 0 on all axes about 10% of the time when using the INSTANT_ON mode. The final answer suggests that the HIGHEST PEAK DATA value is only updated once the sensor returns to inactive mode (bit 4 of the ACTIVITY_STATUS register). The user's observation of high acceleration values during the 100ms wait period supports this explanation.
AI Generated Content
Category: Hardware
Product Number: ADXL372

I'm trying to use the chip to detect shocks and their maximum values ​​using the HIGHEST PEAK DATA registers and the INSTANT_ON mode.

Most of the time it works, but sometimes (~ 1 time out of 10), all 3 max peak values ​​are 0.

Below is my chip register configuration:

Reg 0x04 = 0x0
Reg 0x05 = 0x0
Reg 0x20 = 0x0
Reg 0x21 = 0x0
Reg 0x22 = 0x0
Reg 0x23 = 0xC
Reg 0x24 = 0x81
Reg 0x25 = 0xC
Reg 0x26 = 0x81
Reg 0x27 = 0xC
Reg 0x28 = 0x81
Reg 0x29 = 0x0
Reg 0x2A = 0xC
Reg 0x2B = 0x81
Reg 0x2C = 0xC
Reg 0x2D = 0x81
Reg 0x2E = 0xC
Reg 0x2F = 0x81
Reg 0x30 = 0x0
Reg 0x31 = 0x2
Reg 0x32 = 0x0
Reg 0x33 = 0x0
Reg 0x34 = 0x0
Reg 0x35 = 0x0
Reg 0x36 = 0x0
Reg 0x37 = 0x0
Reg 0x38 = 0x2
Reg 0x39 = 0xFD
Reg 0x3A = 0x39
Reg 0x3B = 0x40
Reg 0x3C = 0x0
Reg 0x3D = 0x80
Reg 0x3E = 0x24
Reg 0x3F = 0x1A

When the interrupt line INT1 goes high, I read the activity status register and if activity is detected (bit 5), I wait 100ms before reading the Highest_Peak registers. Then I put the chip back into INSTANT_ON mode.

The shocks are correctly detected, the chip wakes up and the activity bit goes to 1, but sometimes (~1 time out of 10) reading the HIGHEST_PEAK registers returns 0 on all 3 axes.

To pinpoint the problem, I added acceleration readings during the 100ms wait (~1 reading of the 3 axes every 1.3ms).

Below are the results of a shock with functional MAX_PEAKS detection followed by a shock with MAX_PEAKS set to 0. (There are 66 times the acceleration values ​​in g read at 1.3ms, followed by the highest_peaks values.)

-7.30, -12.40, -24.60
-8.40, -4.90, -18.60
-1.60, 1.30, -9.20
-1.50, 4.10, -0.70
1.30, 0.20, 4.30
3.60, -3.90, 3.30
7.10, -3.40, 2.10
8.30, -2.60, -3.30
4.20, 5.10, -9.50
0.90, 2.00, -9.20
-1.60, -1.90, 0.70
1.60, -2.10, 3.50
4.90, 1.20, 8.30
1.80, 2.10, 10.00
-1.80, -1.10, 3.50
-3.50, 1.40, -2.00
-1.60, 2.90, -1.00
-1.60, -2.30, 3.90
-0.80, 1.70, 1.40
1.80, 1.40, -0.70
0.00, -3.50, 1.00
-1.90, -0.60, 4.20
0.30, 1.60, 5.00
0.30, -0.20, 1.20
0.80, -0.70, -1.10
1.80, -0.30, 0.40
-0.50, 1.40, 2.70
-1.10, -0.20, 2.30
0.70, -1.10, 0.70
1.30, 0.70, -0.30
-0.90, 1.10, 0.30
-1.80, -0.70, 0.30
0.20, -0.50, 1.60
1.30, -0.20, 2.20
0.50, 0.00, 0.80
-1.10, -0.30, -0.80
0.30, 0.20, 0.00
0.40, -0.10, 1.00
0.70, -0.20, 0.20
-0.50, -0.30, -0.50
-0.10, -0.50, -0.50
0.20, 0.30, -0.60
-1.00, 0.20, -0.10
-0.50, -0.80, 1.20
0.30, 0.30, 0.30
0.90, 0.30, -0.30
-0.40, -0.50, -0.20
-1.10, -0.20, 0.00
0.20, 0.70, -0.60
1.10, 1.50, -2.80
0.10, 0.90, -4.50
2.40, 0.60, -2.20
2.20, -0.30, 0.50
1.60, -0.80, 2.10
-1.30, -0.40, 1.00
-0.90, 1.00, 0.70
0.00, -0.10, 1.10
-2.10, 0.00, 1.10
-1.30, -0.60, -0.60
1.10, -0.10, 1.20
-1.20, 0.10, 0.60
0.00, 0.20, 0.80
-0.30, 0.30, 0.00
0.00, -0.40, -0.20
-1.00, 0.20, -0.30
0.50, 0.80, -0.60
Max peak
Acc X : -10.10 g
Acc Y : -9.90 g
Acc Z : -25.40 g

-19.00, -34.90, -69.00
-8.40, -9.20, -94.40
-11.30, 1.20, -85.90
8.70, -7.20, -17.40
3.90, 2.20, 17.30
3.60, 11.20, 56.00
9.80, 6.90, 65.50
11.40, 7.20, 39.30
0.40, -5.40, 3.40
-3.70, -1.00, -16.90
0.30, 8.80, -13.80
0.80, 8.50, 6.80
0.10, 6.10, 21.20
-3.00, 2.00, 24.10
0.50, -1.40, 13.50
2.40, 1.30, -4.20
2.40, 2.60, -11.10
4.90, -0.10, -2.60
3.90, -1.60, 6.90
-2.20, 3.60, 2.50
-3.60, 4.20, 0.70
4.40, 1.30, 0.00
-0.70, -4.10, 5.00
-2.90, -1.30, 8.60
0.90, -0.10, 6.80
-1.60, -1.00, 1.70
0.60, -0.30, 0.80
1.60, 0.20, 3.20
-0.10, 1.10, 7.10
-3.60, 0.10, 7.20
-1.30, -0.50, 4.10
0.20, 0.60, 0.80
0.60, 1.00, 1.20
0.60, 0.50, 2.30
-1.10, 0.50, 2.90
-0.20, 0.40, 2.40
-1.00, -0.10, -0.60
-2.20, -0.30, -4.00
0.50, -1.10, -11.30
-3.90, 1.80, -6.60
-4.00, -0.80, 1.40
-0.60, -1.70, 2.90
3.20, -1.00, 1.30
3.10, 0.10, -0.10
1.00, -0.70, 0.50
-0.80, -0.50, 2.40
1.00, -0.10, 3.90
-0.40, -0.50, 1.80
-1.10, -0.40, -0.10
1.60, -0.70, 0.50
1.10, 0.00, 1.50
-0.90, 0.10, 1.30
-0.70, -0.10, 0.90
0.10, -0.60, 0.60
1.40, -0.20, 0.10
0.00, 0.40, -0.20
-0.60, 0.00, 0.90
0.70, -1.00, 0.90
-0.80, -0.60, -0.30
-0.20, -0.20, 0.60
0.40, -0.30, 1.00
-1.20, 0.40, 0.30
-0.30, 0.30, -0.10
0.00, -0.30, 0.10
-1.50, -0.20, 0.50
-0.60, -0.10, 0.50
Max peak
Acc X : 0.00 g
Acc Y : 0.00 g
Acc Z : 0.00 g



When the problem appears, we can see that many measurements are above 10g (threshold defined for Active).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.