Post Go back to editing

About CLK Frequency of ADXL366

Thread Summary

The user asked about the CLK frequency of the ADXL366 for SPI communication at VDD 1.8V. The final answer confirms that SPI can run at 8 MHz, but warns of potential output offset if other devices on the SPI bus operate at significantly higher speeds. Supplying the V_reg pin with its own voltage can reduce this offset.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADXL366

Hi,

Please tell me about the CLK frequency of the ADXL366.
Is it possible to use an 8 MHz clock for SPI communication under VDD 1.8 V conditions?

VDD 2V: 8 MHz
1.2V < VDDIO < 1.4V: 5 MHz
1.1V < VDDIO < 1.2V: 2.5 MHz
The specifications listed above are available, but could you please provide the clock specifications for the 1.8V operating condition?

Best Regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.