ADXL366
Recommended for New Designs
The ADXL366 is an ultra-low power, 3-axis microelectromechanical
systems (MEMS) accelerometer that consumes only 0.96μA at a
100Hz output data rate (ODR...
Datasheet
ADXL366 on Analog.com
Hi,
Please tell me about the CLK frequency of the ADXL366.
Is it possible to use an 8 MHz clock for SPI communication under VDD 1.8 V conditions?

VDD 2V: 8 MHz
1.2V < VDDIO < 1.4V: 5 MHz
1.1V < VDDIO < 1.2V: 2.5 MHz
The specifications listed above are available, but could you please provide the clock specifications for the 1.8V operating condition?
Best Regards,
Hi there, thanks for your question. I've spoken to the evaluation team and they have told me that SPI can run at 8 MHz under these conditions, but a high clock speed may introduce an offset to the output if there is another device on the SPI bus streaming at significantly higher speeds than the XL366. If this is the case for your application, it may be worth following the SPI bus sharing layout example from the datasheet:

Hope this is helpful to your design process.
Regards,
Nico
Hi there, thanks for your question. I've spoken to the evaluation team and they have told me that SPI can run at 8 MHz under these conditions, but a high clock speed may introduce an offset to the output if there is another device on the SPI bus streaming at significantly higher speeds than the XL366. If this is the case for your application, it may be worth following the SPI bus sharing layout example from the datasheet:

Hope this is helpful to your design process.
Regards,
Nico