Post Go back to editing

ADXL380 operating temperature range

Thread Summary

The user inquired about the correct operating temperature range for the ADXL380, noting discrepancies across different sources. The final answer confirms the correct range is -40 to 125 °C, as stated in the datasheet, following a product change notice that extended the upper limit from 85 to 125 °C.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADXL380

I see contradicting information on the operating temperature range of the ADXL380. What is the correct range?

* Datasheet says -40 to 125 °C on first page features and last page ordering guide

* Accelerometer selection table says 85 to 125 °C
 

* Product page says -40 to 85 °C

  • Hi there, thanks for pointing this out. We're now in the process of fixing the discrepancy across ADI services; the actual operating range should be -40 to 125 ºC. There was a product change notice (PCN) in October of last year that extended the upper end of the temperature range from 85 to 125 ºC, and some sites may not have been updated to reflect this. The datasheet value is the correct range.