Post Go back to editing

Setup LTM2985 with 2x PT100 RTD and 1kΩ shared RSense in 2-Wire-Mode

Thread Summary

The user encountered incorrect and drifting data when setting up the LTC2985 with two PT100 RTDs in 2-Wire-Mode with a shared 1 kΩ RSense. The issue was resolved by correctly assigning the data to channels CH6 and CH10 instead of CH5 and CH9.
AI Generated Content
Category: Hardware
Product Number: LTM2985

Hello ADI,

I have trouble setting up the LTM2985 with two PT100 RTDs. They have a shared RSense of 1 kΩ and are configured in 2-Wire-Mode. My schematic is very close to figure 12, "Shared 2-Wire RTD Example" in the LTC2985 Datasheet (Rev. A) on pages 39 and 40. To illustrate my problem, I have copied the two pages and put my values in.

Two thermocouples are already working without a cold junction. The RTDs will be used for that. At the moment I use the minimal example with the RTDs and the RSense only.

The data I get is extremely wrong and continuously drifting away. I searched for a very long time and don't get the problem. Please help.

Kind regards,
Mario 

Here is the Data I get.

| Time(sec) | CH5 ResultReg | CH5 Status | CH5 Wert | CH9 ResultReg | Status | Wert     |
|-----------|---------------|------------|----------|---------------|--------|----------|
| 0         | 05FCC043      | 5          | 16176,07 | 01FEEB86      | 1      | 16314,88 |
| 2,564     | 05FCAF99      | 5          | 16171,9  | 01FEC3CE      | 1      | 16304,95 |
| 3,065     | 05FCADC3      | 5          | 16171,44 | 01FEBECF      | 1      | 16303,7  |
| 3,589     | 05FCA993      | 5          | 16170,39 | 01FEB568      | 1      | 16301,35 |
| 4,092     | 05FCA7B8      | 5          | 16169,93 | 01FEB0EB      | 1      | 16300,23 |
| 4,553     | 05FCA5BD      | 5          | 16169,43 | 01FEAC02      | 1      | 16299    |
| 5,008     | 05FCA18D      | 5          | 16168,39 | 01FEA292      | 1      | 16296,64 |
| 5,459     | 05FC9F9C      | 5          | 16167,9  | 01FE9E0F      | 1      | 16295,51 |
| 5,906     | 05FC9D9D      | 5          | 16167,4  | 01FE9980      | 1      | 16294,38 |
| 6,369     | 05FC99E8      | 5          | 16166,48 | 01FE9042      | 1      | 16292,06 |
| 6,874     | 05FC97E6      | 5          | 16165,97 | 01FE8BB8      | 1      | 16290,93 |
| 7,365     | 05FC93B8      | 5          | 16164,93 | 01FE82F3      | 1      | 16288,74 |
| 7,885     | 05FC921D      | 5          | 16164,53 | 01FE7E46      | 1      | 16287,57 |
| 8,325     | 05FC8FD3      | 5          | 16163,96 | 01FE79FC      | 1      | 16286,5  |
| 8,842     | 05FC8C7F      | 5          | 16163,12 | 01FE7176      | 1      | 16284,37 |
| 9,326     | 05FC8A31      | 5          | 16162,55 | 01FE6D0A      | 1      | 16283,26 |
| 9,831     | 05FC8682      | 5          | 16161,63 | 01FE6413      | 1      | 16281,02 |
| 10,346    | 05FC849B      | 5          | 16161,15 | 01FE6037      | 1      | 16280,05 |
| 10,825    | 05FC80DD      | 5          | 16160,22 | 01FE57A9      | 1      | 16277,92 |
| 11,296    | 05FC7F1F      | 5          | 16159,78 | 01FE53D8      | 1      | 16276,96 |
| 11,796    | 05FC7B53      | 5          | 16158,83 | 01FE4B26      | 1      | 16274,79 |
| 12,246    | 05FC7994      | 5          | 16158,39 | 01FE4735      | 1      | 16273,8  |
| 12,678    | 05FC77AF      | 5          | 16157,92 | 01FE4357      | 1      | 16272,83 |
| 13,176    | 05FC742F      | 5          | 16157,05 | 01FE3AE2      | 1      | 16270,72 |
| 13,678    | 05FC72AF      | 5          | 16156,67 | 01FE3782      | 1      | 16269,88 |
| 14,113    | 05FC70F0      | 5          | 16156,23 | 01FE33D6      | 1      | 16268,96 |
| 14,633    | 05FC6D73      | 5          | 16155,36 | 01FE2BC7      | 1      | 16266,94 |
| 15,126    | 05FC6BAC      | 5          | 16154,92 | 01FE2835      | 1      | 16266,05 |
| 15,576    | 05FC6844      | 5          | 16154,07 | 01FE209B      | 1      | 16264,15 |
| 16,093    | 05FC66C2      | 5          | 16153,69 | 01FE1CCE      | 1      | 16263,2  |
| 16,555    | 05FC649F      | 5          | 16153,16 | 01FE18E2      | 1      | 16262,22 |
| 17,034    | 05FC614F      | 5          | 16152,33 | 01FE1172      | 1      | 16260,36 |
| 17,542    | 05FC5F89      | 5          | 16151,88 | 01FE0DB4      | 1      | 16259,43 |
| 18,017    | 05FC5C52      | 5          | 16151,08 | 01FE0649      | 1      | 16257,57 |
| 18,481    | 05FC5A9F      | 5          | 16150,66 | 01FE02E6      | 1      | 16256,72 |
| 18,969    | 05FC5725      | 5          | 16149,79 | 01FDFBDC      | 1      | 16254,96 |
| 19,452    | 05FC557D      | 5          | 16149,37 | 01FDF849      | 1      | 16254,07 |
| 19,974    | 05FC53C8      | 5          | 16148,95 | 01FDF472      | 1      | 16253,11 |
| 20,446    | 05FC50E3      | 5          | 16148,22 | 01FDEDF0      | 1      | 16251,48 |
| 20,936    | 05FC4F12      | 5          | 16147,77 | 01FDEA77      | 1      | 16250,62 |
| 21,407    | 05FC4BBC      | 5          | 16146,93 | 01FDE32C      | 1      | 16248,79 |
| 21,894    | 05FC4A6E      | 5          | 16146,61 | 01FDE017      | 1      | 16248,02 |
| 22,314    | 85F06400      | 133        | 15385    | 01FDDCB5      | 1      | 16247,18 |
| 22,806    | 85F06400      | 133        | 15385    | 01FDD624      | 1      | 16245,54 |
| 23,281    | 85F06400      | 133        | 15385    | 01FDD30B      | 1      | 16244,76 |
| 23,783    | 85F06400      | 133        | 15385    | 01FDCC41      | 1      | 16243,06 |
| 24,262    | 85F06400      | 133        | 15385    | 01FDC901      | 1      | 16242,25 |
| 24,781    | 85F06400      | 133        | 15385    | 01FDC29B      | 1      | 16240,65 |
| 25,523    | 85F06400      | 133        | 15385    | 01FDBC33      | 1      | 16239,05 |
| 26,011    | 85F06400      | 133        | 15385    | 01FDB906      | 1      | 16238,26 |
| 26,796    | 85F06400      | 133        | 15385    | 01FDB2A9      | 1      | 16236,67 |

The plotted data looks like this.


Parents Reply Children
No Data