Post Go back to editing

Cost-effective hermetic sealed accelerometers

Thread Summary

The user seeks a cost-effective, hermetically sealed accelerometer with AEC, >1kHz bandwidth, 3-16g range, and digital (I2C/SPI) interface. The ADXL358 and ADXL359 are cost-effective alternatives but are not hermetically sealed. The ADXL100x family has analog output and wider bandwidth, making them less suitable. Hermetic sealing is a significant cost factor.
AI Generated Content
Category: Hardware
Product Number: ADXL354

Hello, 

I'm looking for a more cost effective version of the ADXL354. I don't need the 20 bit resolution. The adxl312 is more appropriate for my application, but the DS doesn't indicate it's hermetically sealed. Is there a more cost-effective accerlerometer with AEC, > 1kHz bandwidth, range 3-16g, and digital (I2C / SPI) interface?

  • Hello  I am afraid that ADXL312 is not sealed. The cost-effective alternatives in the ADXL35x family are ADXL358 and ADXL359 but they also come on a non-hermetic plastic package.

    You can check the ADXL100x family but they are analog output and suited for wider BW.

    The ceramic package and making the part hermetically sealed is one of the reasons that make these products more expensive to produce rather than the ASIC itself. 

    hope this info helps in any case,

    Mario SM