ADPD188BI
Recommended for New Designs
The ADPD188BI is a complete photometric system for smoke
detection using optical dual wavelength technology. The module integrates a highly efficient photometric...
Datasheet
ADPD188BI on Analog.com
We are currently evaluating the ADPD188BI sensor for smoke detection applications and are using the smoke detection configuration provided in the official Analog Devices driver repository.
We have successfully initialized the device and are able to read sensor data over I2C. The sensor appears operational, and FIFO/sample reads are functioning correctly. However, when the sensor is exposed to smoke, we are not observing any noticeable change in the blue or IR measurement values.
Our setup is based closely on the provided smoke_detect_setup() example configuration from the ADPD188 driver library. We are using: