When using the ADXL355 in EXT_SYNC = 10, EXT_CLK = 0 — External Synchronization With Interpolation mode, is it possible to set the following:
Name: Filter, Address: 0x28, Data: 0x02 (1000 Hz and 250 Hz settings)?
(If EXT_SYNC = 01, ODR is fixed at 4KHz, but if EXT_SYNC = 10, EXT_CLK = 0, is it correct that ODR can be set to a frequency other than 4KHz?)
Currently, the ADXL355 has the following settings:
• Name: Range, Address: 0x2C, Data: 0x82 (4G setting)
• Name: Filter, Address: 0x28, Data: 0x02 (1000 Hz and 250 Hz settings)
• Name: Sync, Address: 0x2B, Data: 0x02 (EXT_CLK=0, external sync, interpolation filter)
We are seeing an output that looks like aliasing noise around 600Hz, and we would like to confirm whether the filter is working. We apologize for the inconvenience, but we would appreciate your assistance.