I need to capture shock windows into the sensor's FIFO triggered by a fast shock over a high g-threshold.
FIFO is set to triggered mode.
The ODR is 3200Hz and I would like to configure the low-pass antialiasing filter to 200Hz.
It seems that when the sensor's low-pass activity filter (10Hz) is enabled, the antialiasing filter is also enabled.
When the activity filter is disabled, the antialiasing filter is also disabled.
The datasheet recommends turning the activity filter off for high g-events.
Is it possible to only have the antialiasing filter (200Hz) enabled without the activity filter?
Best regards,
VN