Post Go back to editing

why pin 1 marker on bottom of adxl367bccz-rl7?

Category: Hardware
Product Number: ADXL367

Howdy,

I'm wondering why the pin 1 marker is only the bottom of the sensor instead of on both the bottom and top? I had some prototype boards assembled, and the adxl367 was not working. I suspected an orientation issue, but the only way I could truly confirm it was by heat gunning the adxl367 off a board. Since I don't have a reflow station, I had to trash a board to verify that the pin 1 was rotated 180 degrees from where it should be. Also I did several days of writing software tests.

I don't know if you all agree, but I wish AD would laser etch the pin 1 marker on the top and the bottom. It would be helpful to have the top marker as well. The top marker if etched would probably have survived on several of the prototypes, and I would have been able to confirm the issue right away.

Thanks,
--jim

Parents
  • Hi Jim, thanks for reaching out. Sorry to hear you're having this trouble, this sounds like a frustrating issue. As far as I'm aware, the ADXL367BCCZ-RL7 should have a pin marker etched on the top of the chip. Do you mind sharing some pictures of the chip, as well as where you sourced it from? This will help me track down the issue and confirm why these chips are missing a pin 1 marker, as I've checked the design files and it definitely should.

    Thanks,

    Nico

  • Hi Nico,
    Actually that dot may be the pin1 marker? The pin 1 is in that corner. It looked like a copyright symbol or something.
    PCBWay assembly sourced it. I asked them where they sourced it, and they did send me a packing slip, but the lot number was redacted for some reason. Date code: 2238, Country of assembly: S. Korea, MFG No: ADXL367BCCZ-RL7. 
    --jim

    adxl367 top view

Reply
  • Hi Nico,
    Actually that dot may be the pin1 marker? The pin 1 is in that corner. It looked like a copyright symbol or something.
    PCBWay assembly sourced it. I asked them where they sourced it, and they did send me a packing slip, but the lot number was redacted for some reason. Date code: 2238, Country of assembly: S. Korea, MFG No: ADXL367BCCZ-RL7. 
    --jim

    adxl367 top view

Children