Post Go back to editing

Inquiry Regarding Orientation-Dependent Performance of ADIS16467

Thread Summary

The user inquired about the ADIS16467 sensor's measurement accuracy on a moving platform like a drone. The final answer confirms that the sensor's orientation does not degrade performance, but factors like temperature variations, vibration, and nonlinearities can affect accuracy. The datasheet provides in-run bias stability, angular random walk, and Allan Variance plots to help assess performance under different conditions.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADIS16467

Dear

I would like to inquire about the operating conditions of the ADIS16467 sensor.

If the sensor is mounted on a moving platform such as a drone, does it maintain the specified measurement accuracy (as stated in the datasheet) regardless of its orientation?

Since the sensor is based on MEMS technology, I would like to confirm whether its specified measurement accuracy is preserved under arbitrary attitude and orientation conditions.

Thank you for your support.

  • Dear Bob,

    Thank you for your question. Our IMUs include several parameters in the datasheet specified under standard test conditions that can influence the measurement output and, ultimately, the system‑level performance. Among the most relevant are in‑run bias stability, angular random walk, and other noise and stability‑related metrics that describe the sensor’s behavior over time. The datasheet also provides Allan Variance (AVAR) plots, which visually illustrate these noise characteristics and help identify which error sources dominate at different integration times.

    Temperature variations, vibration transmitted through the structure where the IMU is mounted, and inherent nonlinearities are common contributors to bias in the output measurements and therefore to overall attitude accuracy. The orientation of the IMU within the frame does not degrade its performance; however, the operating conditions of the IMU do have a direct impact.

    Could you please provide more details on the specific parameters you are interested in for your application?

    Kind regards,
    Ruben

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.