Post Go back to editing

Humidity-related output shift on ADXL343 during tilt detection

Thread Summary

The user observed a persistent shift in the Z-axis output of the ADXL343 when exposed to high humidity, which was only resolved after thermal exposure at 60°C. The issue is suspected to be due to moisture absorption in the plastic package, altering the mechanical force profile on the sensing die. A coating material can help insulate the part, and the ADXL355/7B with a hermetic ceramic package is recommended for better humidity resistance.
AI Generated Content
Category: Hardware
Product Number: ADXL343

I am using the ADXL343 for a simple tilt detection application.

This is a threshold-based tilt detection.
The Z-axis output measured at 80° is stored as a reference, and the current Z-axis value is compared against it during operation.

When the device was operated in a high-humidity environment, a significant shift in the Z-axis output was observed.
As a result, tilt was detected at angles lower than expected(e.g., around 75°).

After returning the device to a low-humidity environment, the output shift remained.
However, after leaving the device overnight at approximately 60 °C, the output behavior recovered and tilt detection again occurred around 80°.

This behavior suggests that exposure to high humidity caused a persistent change affecting the Z-axis output, which remained even after humidity was reduced and was only resolved after thermal exposure.

If anyone has insight into physical or electrical mechanisms that could explain such humidity-related output shifts in the ADXL343—whether related to the sensor itself, packaging, or external conditions—I would appreciate your thoughts or experience.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.